DOUT#.SOURCE
Description
Gets or sets the digital output source.
| Value | Description |
|---|---|
| 0 - User | User controls the output value using DOUT#.STATEU |
| 1 - Action Table | Action table controls the output value |
| 2 - FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Fieldbus controls the output value |
Examples
Usage
When DOUT#.SOURCE = 0 (User), then DOUT#.STATE will be controlled by DOUT#.STATEU.
When DOUT#.SOURCE = 1 (Action table), then DOUT#.STATE will be controlled by the assigned action, if any.
When DOUT#.SOURCE = 2 (Fieldbus), then DOUT#.STATE will be controlled by the fieldbus output control object 3601h sub 1.
Code
Changing output state with STATEU and then changing SOURCE to be action table with no action configured:
--> DOUT1.SOURCE 0 //user --> DOUT1.STATE 0 --> DOUT1.STATEU 1 --> DOUT1.STATE 1 --> DOUT1.SOURCE 1 //action table --> DOUT1.STATE 0
Context
For more information see Digital I/O.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 2 |
| Default Value | 0 |
| Data Type | Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | DOUT1.SOURCE | 0x360A | 0x1 | USINT | - | - | RW | False |
| DOUT2.SOURCE | 0x360B | 0x1 | USINT | - | - | RW | False | |
| DOUT3.SOURCE | 0x360C | 0x1 | USINT | - | - | RW | False | |
| DOUT4.SOURCE | 0x360D | 0x1 | USINT | - | - | RW | False | |
| DOUT5.SOURCE | 0x360E | 0x1 | USINT | - | - | RW | False | |
| DOUT6.SOURCE | 0x360F | 0x1 | USINT | - | - | RW | False | |
| DOUT7.SOURCE | 0x3610 | 0x1 | USINT | - | - | RW | False | |
| DOUT8.SOURCE | 0x3611 | 0x1 | USINT | - | - | RW | False | |
| DOUT9.SOURCE | 0x3612 | 0x1 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|